cancel
Showing results for 
Search instead for 
Did you mean: 

STMTouch & Shield

msinger
Associate
Posted on January 09, 2014 at 21:26

What exactly does marking a pin as SHIELD do?

#tsi-stmtouch
1 REPLY 1
Thierry GUILHOT
ST Employee
Posted on January 16, 2014 at 22:25

The shield pin is used to drive an active shield (also called driven shield) plane.

The principle of a driven shield is to drive the shield plane with the same signal as the

electrode. There are several advantages of using a driven shield instead of a grounded one:

o The parasitic capacitance between the electrode and the shield no longer needs to be

charged. This offers an optimum sensitivity.

o A driven shield is useful for certain applications where shielding may be required to:

  – Protect the touch electrodes from a noise source

  – Remove touch sensitivity from the cable or track between the electrode and the

sensing MCU.

  – Increase system stability and performance when a moving metal part is close to

the electrode.

If you need further information, I invite you to have a look to the AN4312.

What exactly does marking a pin as SHIELD do?