cancel
Showing results for 
Search instead for 
Did you mean: 

USB cdc host can not see device after second connection

kqian
Associate II
Posted on February 06, 2014 at 17:06

I found a weir problem on me usb cdc connection. I have one cdc device and one cdc host. Every time I connected device to host, host looks like find another device (VID:0069h, PID:0063h) and stuck there. I have to unplug and reconnect them to let the host to find the correct device (VID:0932h, PID:0004h). If unplug and reconnect again, the host will see  (VID:0069h, PID:0063h). next reconnect will see the correct one, and so on. 

What is the device (VID:0069h, PID:0063h)? how can I get rid of this device from my host?
0 REPLIES 0