2014-04-23 07:54 AM
Hi all together,
I want to test the TIM_6Steps from the ''STM32F4xx_DSP_StdPeriph_Lib_V1.3.0'' Library with the STM32F4-Discovery-Board which uses the STM32F407VGT6. The compiler does not send any error but I do not get any output signal!!! I have added the code in the appendix. I only use the output PE11 instead of PA10 for TIM1 output Channel3. If someone of you has got any idea what I should do to get the program working, please let me know! Thank you. Best regards, Patrick2014-04-23 08:17 AM
And a very basic ''blinkey'' program on the same board with the same programming environment does work?
JW2014-04-23 08:54 AM
2014-04-23 09:20 AM
It's OK, Clive. In the appended source, PE13 *is* instead of PA10.
The problem may be in the files we don't see, e.g. clock settings, incorrectly linked ISRs, incorrect hardware setting (BKIN pin should be switchable between hi and lo, although the doc doesn't say why and I don't wish to understand it from code), or even lack of basic functionality of the board or programming environment - that's why I asked for the ''blinkey''. JW2014-04-24 12:56 AM
Hi, when I download the Example ''TIM_PWM_Output'' to the board it works pretty fine! After that I have only copied the main.c from the ''TIM_6Step'' to the main of the ''TIM_PWM_Output'' example and it does not work although the startup file and the others are the same as the files from example ''TIM_6Step''.
The other thing is, when I try the ''Complementary output example project'' it also does not work!!! Later I want to go on to produce a three phase sinus modulation, that`s why I thought it would be useful to start with the TIM_6step example! Thank you.2014-04-24 01:05 AM
> the startup file and the others are the same as the files from example ''TIM_6Step''.
I don't know where you took these projects from, but NO, THEY ARE NOT THE SAME. JW2014-04-24 05:14 AM
2014-04-24 06:12 AM
Thanks,
I got it working now. I had to import also the stm32f4xx_it.c file because interrupt handling is concerning on a function written in this file. Thank you. Best regards, Patrick