cancel
Showing results for 
Search instead for 
Did you mean: 

I ported a a firmware from IAR Embedded Workbench to Kiel version 4(stm32l100)

sundar
Associate II
Posted on March 27, 2014 at 08:50

I ported a a firmware from IAR Embedded Workbench to Kiel version 4(stm32l100)

I get this warning after building the project in Kiel but not in IAR Warning: &sharp815-D: type qualifier on return type is meaningless.

extern const LonNvDescription* const LonGetNvTable(void);

extern const LonApiError LonPollNv(const unsigned index);

what is the correct way to define this type of function

#stm32l100 #kiel-version-4
5 REPLIES 5
Posted on March 27, 2014 at 14:34

It does seem a bit odd, is the value returned stored in ROM/FLASH? and unmodifiable for that reason? The Keil forum might be worth a try, I'm sure there are people there who'll argue the C specification, and ordering of const, static, etc with you. What does LINT or MISRA say?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Nickname306_O
Senior
Posted on April 01, 2014 at 10:40

Hello sanil.prem,

The type qualifier “ const � is ignored by the compiler since the return value cannot be const.

You shoud delete it.

Best Regards,

Nouha

I ported a a firmware from IAR Embedded Workbench to Kiel version 4(stm32l100)

I get this warning after building the project in Kiel but not in IAR Warning: #815-D: type qualifier on return type is meaningless.

extern const LonNvDescription* const LonGetNvTable(void);

extern const LonApiError LonPollNv(const unsigned index);

what is the correct way to define this type of function

Andrew Neil
Evangelist
Posted on April 01, 2014 at 22:49

''The Keil forum might be worth a try''

He has already posted exactly the same on the Keil forum - and, unsurprisingly, received much the same answer:

http://www.keil.com/forum/56897/

@Sanil: There is no  requirement on any  compiler to produce any warnings at all - so it should come as no surprise that different compilers, from different vendors, choose to give give some different warnings.

If you want a whole different set of warnings, just try putting this code through GCC...

''

what is the correct way to define this type of function''

Again: what, exactly, do you think ''this type''  of function is? Why do you think the 'const' qualifier is necessary or appropriate? What are you trying to achieve by it?
sundar
Associate II
Posted on April 02, 2014 at 05:47

Hello Nouha ,

Thanks for the info ,.it works fine now ,!(No warnings )

Rergards

Sanil

sundar
Associate II
Posted on April 02, 2014 at 05:57

Hello

0690X0000060ModQAE.gif,

Initially I was in dilemma , was relatively new to IAR when compared to Kiel ,

about that function , my understanding now is 'the function call cannot change the return type ..!)

Regards

Sanil