cancel
Showing results for 
Search instead for 
Did you mean: 

.NET Micro Framework in STM32F429 Discovery Board

jwoh
Associate
Posted on February 07, 2014 at 11:15

Dear

I saw STM32F429 discovery board is MF supported. And I looked up the all functions, and it is not include Ethernet. But, only binary image files are offered on the web site. Is there any way of getting porting source? or anyone who tried to solve the problem adding ethernet to discovery32f429

Regards, Jiwon.

2 REPLIES 2
Posted on February 07, 2014 at 18:50

The real problem here is that SDRAM + LCD + ETHERNET is conflicted at the pin level. This is only going to be resolved with a different board design, with a higher pin count device.

Now you could perhaps attach an SPI ETHERNET board to it, with all the lameness in performance that would introduce.
Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..
Just Matt
Associate III
Posted on February 10, 2014 at 15:25

I second the release of the source~!

(If ST reads the forums)

-Matt