cancel
Showing results for 
Search instead for 
Did you mean: 

STR912 EMI Interface: Chip Select

bruce23
Associate
Posted on February 12, 2014 at 01:22

Hi,

Just a quick question on the EMI Interface and in particular chip selects.  I am going to implement 1 bank of  SRAM on a 16bit multiplexed bus. Obviously only one chip select required and I am using P7.0 (CS0).  That leaves the other 3 EMI CS pins on P7 free.  

Can I use these ports as general IO ports or are they fixed as CS pins when when EMI is implemented?

Cheers

#str912
0 REPLIES 0