cancel
Showing results for 
Search instead for 
Did you mean: 

CAN/USB board

stm322399
Senior
Posted on February 10, 2016 at 17:42

Hi there,

I am looking for a board that is able to run as USB device and has CAN transceivers.

OLIMEXIMO with STM32F103 is exclude because of F103 that cannot run USB and CAN simultaneously (they share some internal resources).

Any other MCU (that does not suffer the same fate) should be OK. The board should be reasonably supported on mid-term (e.g. being available for sale within a few years).

Do some of you have an idea where I can find such a gem ? (I did STFW without success by now).
3 REPLIES 3
Walid FTITI_O
Senior II
Posted on February 10, 2016 at 18:13

Hi gonzalez.laurent,

Yes, you can use one of the STM32F4xx Eval boards available at this

http://www.st.com/stonline/stappl/productcatalog/app?page=partNumberSearchPage&levelid=SS1577&parentid=1199&resourcetype=HW

.

-HANIIBAL-
Posted on February 10, 2016 at 18:16

I've picked up these in the past

http://elty.pl/pl/p/STM32F2x7VGT6-DK-A/347

, not sure of current availability.

I've got these, where the modem plug-in can be left off. CAN and 12V can be supplied via a Molex connector. Currently building with 1MB 405 parts, but the foot print works with the 205, 215 parts.

https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/CAN%20not%20working%20on%20STM32F205%20%28proto%20board%29&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506...

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..
stm322399
Senior
Posted on February 12, 2016 at 08:02

Thanks guys.

Clive,

http://elty.pl/pl/p/STM32F2x7VGT6-DK-A/347

look very good, but availability is questionable.

Hannibal, your link led me to boards having no CAN drivers or having too much features, and probably too expensive/big for my needs.

After having virtually walked though the planet several times, I might stop a my starting point: Olimex has a dirt cheap STM32-P405 that I missed at the beginning of my trip, because I was focused on F105/107.

I hope that the F405 will allow me to use CAN and USB simultaneously.

Cheers.