cancel
Showing results for 
Search instead for 
Did you mean: 

iNemo SWD programming problem

daniel23
Associate II
Posted on April 15, 2015 at 19:50

Hi to all, I'm trying to program my iNemo based custom board with the ST LINK provided with the STM32F4 Discovery. When I try to connect with STM32 ST-Link Utility I get the error: '' Core is held in reset''.

Another trial was to use CoCox, and trying to flashing with it I get (''Error: Flash driver function execute timeout Erase:    [  0%] '').

Any idea to solve the problem? Thanks

#inemo #stlink #stm32f103
1 REPLY 1
Posted on April 15, 2015 at 21:30

Make sure the NRESET pin is disconnected from the F4, then investigate why it might be held low in your design, and check if it is.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..