cancel
Showing results for 
Search instead for 
Did you mean: 

difference between i2c master and slave configuration-stm32f4

mohamad_armoon
Associate III
Posted on March 02, 2014 at 15:36

i wnat to have one slave i2c that receive data that transmit by master.

i wrote the master side, but in the receiver slave i dont know what should i do to get that data in i2c .

if anybody knows how should i do ,

you know, is think this procedure is true :''

The master is initially in master transmit mode by sending a 

http://en.wikipedia.org/wiki/Start_bit

 followed by the 7-bit address of the slave it wishes to communicate with, which is finally followed by a single bit representing whether it wishes to write(0) to or read(1) from the slave.

If the slave exists on the bus then it will respond with an 

http://en.wikipedia.org/wiki/Acknowledgement_%28data_networks%29

 bit (active low for acknowledged) for that address. The master then continues in either transmit or receive mode (according to the read/write bit it sent), and the slave continues in its complementary mode (receive or transmit, respectively).''

i don't know how to implement this in stm32f4.

at least i don't know in slave receiver side. please help me
0 REPLIES 0