2014-03-12 12:32 AM
I am going to use STM32F205 series MCU in my project, because it has two FS USB PHY. I am going to use one PHY as host, another PHY as device. Can USB On-The-Go host and device library(UM1021) support two FS USB PHY simultaneously? If the answer is yes, how can i configure dual FS PHY pins for USB On-The-Go host and device library?
Thanks. #stm32 #library #usb #otg2014-03-13 04:30 AM
Hi
''Can USB On-The-Go host and device library(UM1021) support two FS USB PHY simultaneously? '' I believe it can. '' If the answer is yes, how can i configure dual FS PHY pins for USB On-The-Go host and device library?'' I do not know myself, I have not done it. I liased with a guy who has tried it here : https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fUSB%20OTG%20HS%20Host%20in%20Mode%20FS%20internal%20PHY%20and%20USB%20OTG%20FS%20Device&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E1...2014-03-13 08:53 AM