cancel
Showing results for 
Search instead for 
Did you mean: 

Can USB OTG lib. support two FS USB PHY for STM32F205 ?

anil2
Associate
Posted on March 12, 2014 at 08:32

I am going to use STM32F205 series MCU in my project, because it has two FS USB PHY. I am going to use one PHY as host, another PHY as device. Can USB On-The-Go host and device library(UM1021) support two FS USB PHY simultaneously? If the answer is yes, how can i configure dual FS PHY pins for  USB On-The-Go host and device library?

Thanks.

#stm32 #library #usb #otg
2 REPLIES 2
chen
Associate II
Posted on March 13, 2014 at 12:30

Hi

''Can USB On-The-Go host and device library(UM1021) support two FS USB PHY simultaneously? ''

I believe it can.

'' If the answer is yes, how can i configure dual FS PHY pins for  USB On-The-Go host and device library?''

I do not know myself, I have not done it. I liased with a guy who has tried it here :

https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fUSB%20OTG%20HS%20Host%20in%20Mode%20FS%20internal%20PHY%20and%20USB%20OTG%20FS%20Device&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E1...

Posted on March 13, 2014 at 16:53

Olimex had a 407 board with dual USB configuration, may be that built a demo for that?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..