2014-07-24 03:44 PM
In �?y ADC, I use __IO uint32_t uhADCxConvertedValue, but the re�?ding ch�?nge r�?�?dily even th�?ugh the re�?l v�?lt�?ge d�?es n�?t ch�?nge, which is �?.854�?�?.855.
Ple�?se hel�?2014-07-24 05:02 PM
2014-07-25 04:51 AM
Dear Clive 1
I am using STM32Cube_FW_F4_V1.1.0\Projects\STM32F429I-Discovery\Examples\ADC\ADC_RegularConversion_DMA How to change frequently and sample time? Thanks2014-07-25 05:41 AM
/* ADC Common Init **********************************************************/
ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent; ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2; ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled; ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles; ADC_CommonInit(&ADC_CommonInitStructure); /* ADC3 Init ****************************************************************/ ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; ADC_InitStructure.ADC_ScanConvMode = DISABLE; ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfConversion = 1; ADC_Init(ADC3, &ADC_InitStructure); /* ADC3 regular channel13 configuration *************************************/ ADC_RegularChannelConfig(ADC3, ADC_Channel_13, 1, ADC_SampleTime_3Cycles);2014-07-25 07:09 AM
The example uses ADC3 channel 8 on PF10. On the 429 Disco this pin is dedicated to LCD Enable, with a 4.7K pull down resister. Did you modify the example to use one of the 3 freely available ADC channels ?
Cheers, Hal2014-07-26 03:11 AM
Thanks for help.
I change ADC3 channel 8 to PC3. I feel something wrong here. The voltage being monitored is around 1.4v, but once connect with PC3, the voltage drop to to 0.8v. How to fix it? Thanks2014-07-26 04:13 AM
How to fix it?
Use an OpAmp, or otherwise figure out why your signal is incapable of providing sufficient current into the unbuffered input. What ishttp://www.planetanalog.com/author.asp?section_id=510&doc_id=559252
?