cancel
Showing results for 
Search instead for 
Did you mean: 

emulate VisualStudio/Atmel Studio features with Keil uVision

stanzanim
Associate III
Posted on August 05, 2015 at 10:06

hello forum

I started using uVision with STM32 L0 coming from Atmel Studio development environment. Withoud giving any comparative opinion among the two environment, I just complain about the fact that uVision does not provide a relase and a debug configuratio ready to use. It is comfortable having a debug setup with the proper compiler and linker options already there.

any comments?

thanks

1 REPLY 1
tm3341
Associate II
Posted on August 05, 2015 at 10:25

You can still create 2 targets in single project, set them different options (debug/release) and save your project template forever. When you start new project, just copy/paste template and start!