cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 different run from chip vs Debugger

isaac
Associate II
Posted on January 23, 2015 at 01:27

An application which includes DMA over SPI communication protocol is running nicely once STM32F405 is powered up. However, once running the same code from debugger - it does NOT behave properly.

What might be the cause(s) for the difference?

Some more info: The debugger is an IAR I-jet and the development tool is Workbench IDE 7.30. CPU system clock is 36MHz from the HSI. 

#stm32f4-debugger-initialization
0 REPLIES 0