cancel
Showing results for 
Search instead for 
Did you mean: 

Does USB OTG Require Pullup on DP line?

Rogers.Gary
Senior II
Posted on November 02, 2015 at 05:02

Does the Discovery board use pull-up or pull-down resistors on the USB OTG?

Schematic says it doesn't, the USB standard says it's required.

Any guesses?

Thanks...

1 REPLY 1
Amel NASRI
ST Employee
Posted on November 10, 2015 at 12:07

Hi roofie01,

There are internal pullup available within the USB peripheral. So there is no need to add external ones.

This what explains why you don't see them in discovery board schematic.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.