cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F746G-DISCO - fail RESERVED BITS when copy bin from mbed

domanski0karol
Associate III
Posted on June 28, 2016 at 09:51

Hi, I have a problem with my stm32f46g disco board. When I want to compile program on mbed.org and after that copy that file to disco board I get a fail.txt and info: RESERVED BITS. What happen? I may connect with ST-Link, its connects without problem.

09:48:33 : ST-LINK SN : 066AFF525053885087033137

09:48:33 : ST-LINK Firmware version : V2J23M7

09:48:33 : Connected via SWD.

09:48:33 : SWD Frequency = 1,8 MHz.

09:48:33 : Connection mode : Normal.

09:48:33 : Device ID:0x449

09:48:33 : Device family :STM32F7xx

0690X00000605QNQAY.png

#stm32f7
2 REPLIES 2
Nesrine M_O
Lead II
Posted on June 29, 2016 at 13:04

Hi karol.karol,

May be you can get more help about this issue in

https://developer.mbed.org/forum/

forum 

-Syrine-

Posted on June 29, 2016 at 13:33

Or perhaps start by getting the most current firmware on the ST-LINK?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..