cancel
Showing results for 
Search instead for 
Did you mean: 

VCP Demo Project Available with STM32_USB-FS-Device_Lib_V4.0.0 Not Working

1605mystery
Associate II
Posted on April 09, 2014 at 13:16

Hi Guys,

I am trying to run VCP project on STM32F103RET6 after some modification it's not working fine.

Modification done are

1) Not configured USB disconnect pin as I don't have one in my Eval kit.

2) HSE configuration to 16MHz as am using external oscillator of 16MHz.

3) USB PLL Clock is configured for 48MHz.

Still the demo project isn't working. USB ISR get's executed and also at times USB status (bDeviceState) is attached . Still I don't see same on my PC side.

Can anyone suggest me for same ?

Regards

,

 

Omji Mishra
1 REPLY 1
Posted on April 09, 2014 at 13:38

[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Virtual%20Com%20Port%20for%20STM32F103XC&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx&currentviews=46]Previous, related thread

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..