cancel
Showing results for 
Search instead for 
Did you mean: 

error while compiling the stm discovery-kit touch example

ahmadaneequekhalid
Associate
Posted on April 29, 2014 at 08:45

hi,

 i am working on touch interface for start i am trying to work on stm discovery board. i have downloaded the touch example provided by the st.com while compiling the project i am facing the problems

stm8_tsl_rc_acquisition.c  

Error[As011]: Undefined symbol: EndWaitForVih E:\Ahmad\PRJ_WHITE\touch\an3279\Libraries\STM8_TouchSensing_Driver\src\stm8_tsl_rc_acquisition.c 366 

Error[As011]: Undefined symbol: EndWaitForVih E:\Ahmad\PRJ_WHITE\touch\an3279\Libraries\STM8_TouchSensing_Driver\src\stm8_tsl_rc_acquisition.c 366 

Error[As011]: Undefined symbol: EndWaitForVih E:\Ahmad\PRJ_WHITE\touch\an3279\Libraries\STM8_TouchSensing_Driver\src\stm8_tsl_rc_acquisition.c 366 

Error[As011]: Undefined symbol: WaitForVih E:\Ahmad\PRJ_WHITE\touch\an3279\Libraries\STM8_TouchSensing_Driver\src\stm8_tsl_rc_acquisition.c 369 

Error[As011]: Undefined symbol: WaitForVih E:\Ahmad\PRJ_WHITE\touch\an3279\Libraries\STM8_TouchSensing_Driver\src\stm8_tsl_rc_acquisition.c 369 

Error[As011]: Undefined symbol: WaitForVih E:\Ahmad\PRJ_WHITE\touch\an3279\Libraries\STM8_TouchSensing_Driver\src\stm8_tsl_rc_acquisition.c 369 

Error[Og010]: Inline assembler instruction does not have a unique size: ''        bcp a, (x)'' E:\Ahmad\PRJ_WHITE\touch\an3279\Libraries\STM8_TouchSensing_Driver\src\stm8_tsl_rc_acquisition.c 301 

Error[As011]: Undefined symbol: EndWaitForVil E:\Ahmad\PRJ_WHITE\touch\an3279\Libraries\STM8_TouchSensing_Driver\src\stm8_tsl_rc_acquisition.c 302 

Error[As011]: Undefined symbol: EndWaitForVil E:\Ahmad\PRJ_WHITE\touch\an3279\Libraries\STM8_TouchSensing_Driver\src\stm8_tsl_rc_acquisition.c 302 

Error[As011]: Undefined symbol: EndWaitForVil E:\Ahmad\PRJ_WHITE\touch\an3279\Libraries\STM8_TouchSensing_Driver\src\stm8_tsl_rc_acquisition.c 302 

Error[As011]: Undefined symbol: WaitForVil E:\Ahmad\PRJ_WHITE\touch\an3279\Libraries\STM8_TouchSensing_Driver\src\stm8_tsl_rc_acquisition.c 305 

Error[As011]: Undefined symbol: WaitForVil E:\Ahmad\PRJ_WHITE\touch\an3279\Libraries\STM8_TouchSensing_Driver\src\stm8_tsl_rc_acquisition.c 305 

Error[As011]: Undefined symbol: WaitForVil E:\Ahmad\PRJ_WHITE\touch\an3279\Libraries\STM8_TouchSensing_Driver\src\stm8_tsl_rc_acquisition.c 305 

Error[As011]: Undefined symbol: ShiftLoopVih E:\Ahmad\PRJ_WHITE\touch\an3279\Libraries\STM8_TouchSensing_Driver\src\stm8_tsl_rc_acquisition.c 251 

Error[As011]: Undefined symbol: ShiftLoopVih E:\Ahmad\PRJ_WHITE\touch\an3279\Libraries\STM8_TouchSensing_Driver\src\stm8_tsl_rc_acquisition.c 251 

Error[As011]: Undefined symbol: ShiftLoopVih E:\Ahmad\PRJ_WHITE\touch\an3279\Libraries\STM8_TouchSensing_Driver\src\stm8_tsl_rc_acquisition.c 251 

Tool Internal Error: 

Internal Error: [CoreUtil/General]: Size mismatch for ''        AND       A, (X)'', inserted as 1 bytes, assembled as 3 bytes 

Internal Error: [CoreUtil/General]: Size mismatch for ''        AND       A, (X)'', inserted as 1 bytes, assembled as 3 bytes 

Error while running C/C++ Compiler 

 

Total number of errors: 18 

Total number of warnings: 0 

I have tried to comment the lines but the file is write protected. 

help any one

#discovery-touch-not-compiling
4 REPLIES 4
mike239955_stm1
Associate
Posted on October 08, 2014 at 18:45

Good day,

Did you manage to resolove this problem as I am having the exact same problem?

Regards,

Mike

Andrew Neil
Evangelist
Posted on October 15, 2014 at 20:30

''Error[As011]: Undefined symbol: ...''

So define it, then!

vasily
Associate
Posted on December 09, 2014 at 23:46

I have the same problem. I'm not familiar with this C compiler and especially with asm inlines where it actually fails compiling. In fact, the code is tailored individually for 3 compilers (IAR, COSMIC, RAISONANCE). The IAR is detected correctly but fails compiling. Probably some version incompatibility.

I removed and commented out all the touch sensing code and it compiled and linked.

However, now I don't know how to make an s19 for flashing. Will keep looking.

ag
Associate
Posted on February 01, 2015 at 10:00

Hi, Khalid

Upgrade STM Touch Sensing Driver in project.

Just copy new *.h *.c  over old files in /inc and /src.

If you will upgrade std periph driver too, then also edit stm8s.h:

uncomment  #define STM8S105, rebuild and load project to device.

https://yadi.sk/d/26dA7PMTeP5h4