cancel
Showing results for 
Search instead for 
Did you mean: 

ST-Link + Level 1 read protection = bricked?

gbigden
Associate III
Posted on January 28, 2016 at 14:18

Using IAR EWARM with ST-Link.

I just set the protection level to Level 1 and now I cannot get in again to change the RDPRT  bits back to Level 0

Any suggestions?

#stm32f303x-read-protection
4 REPLIES 4
pkumar1883
Associate II
Posted on January 28, 2016 at 15:00

Just try USART Boot loader and see if it is working. Level 1 protection can not brick it, could be some other reason.

gbigden
Associate III
Posted on January 28, 2016 at 15:13

Unfortunately I do not have access to the USART bootloader pins. Looks like I will have to replace the chip on the board.

Amel NASRI
ST Employee
Posted on January 28, 2016 at 15:15

You can also use

http://www.st.com/web/en/catalog/tools/PF258168

to update protection level and come back to Level0.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

gbigden
Associate III
Posted on January 28, 2016 at 15:37

Thanks! Works perfectly! I am going to add a ''suicide'' command to my prog to change the Level 1 bits to Level 0 to enable me to do this easily from the PC app interface.