2014-05-01 04:26 PM
Hello, we are wanting to call the built-in bootloader from our application without manipulating the BOOT0/BOOT1 pins. I am trying to use the EVAL board to validate our method. The Users Manual for the Eval board does state: ''The RS-232 boot loader mechanism is not supported on the STM32429I-EVAL''. There is no explanation of this statement. However, if I move the Boot0 switch on the eval board to 1 and power cycle, I am able to at least connect to the bootloader over RS-232 using the ST demo flash loader program. If I can get that far by calling the bootloader on the Eval board with the BOOT pins both at 0, I will call it a success until our hardware is ready.
I have tried both calling the bootloader from C code, using the method posted on Youtube, and also calling it from my startup assemble code, using the method Clive has suggested in the forum, as follows (I am using IAR):;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;
;; ;; Default interrupt handlers. ;; THUMB PUBWEAK Reset_Handler SECTION .text:CODE:REORDER:NOROOT(2) Reset_HandlerLDR R0,=0x1FFF0000
LDR R1,[R0,#0] MOV SP,R1 LDR R0,[R0,#4] BX R0 ;debugger shows 0x1FFF4ABF in R0 at this point Unfortunately, both methods display the same behavior - I cannot connect to the bootloader using the demo program. If I use the debugger, I can hit a breakpoint at the start of the bootloader (at 0x1FFF4ABE) , and can trace through it until I get bored, but as soon as I hit run, I hit a breakpoint back at the BX R0 line above, as if a reset is occurring, or the bootloader is jumping back to the start of the application. This made me suspect the dual boot mode of the 429, but I used ST-Link to verify the BFB2 bit in the options byte is cleared, so no dual boot should be taking place. Any ideas?2014-05-01 04:55 PM
Try this
Reboot_Loader PROC
EXPORT Reboot_Loader
LDR R0, =0x40023844 ; RCC_APB2ENR
LDR R1, =0x00004000 ; ENABLE SYSCFG CLOCK
STR R1, [R0, #0]
LDR R0, =0x40013800 ; SYSCFG_MEMRMP
LDR R1, =0x00000001 ; MAP ROM AT ZERO
STR R1, [R0, #0]
LDR R0, =0x1FFF0000 ; ROM BASE
LDR SP,[R0, #0] ; SP @ +0
LDR R0,[R0, #4] ; PC @ +4
BX R0
ENDP ; sourcer32@gmail.com
2014-05-02 09:03 AM
Wow - you are the man, Clive. That worked like a champ. Thank you!
2014-12-01 02:58 AM
Hi Clive
You got me out of the cr@p again! Thanks Andy.2015-07-10 12:32 PM
2015-07-10 01:11 PM
I think I figured this out by adding the following to startup_stm32f429xx.s after the Reset_Handler
Reboot_Loader ;PROC
EXPORT Reboot_Loader
LDR R0, =0x40023844 ; RCC_APB2ENR
LDR R1, =0x00004000 ; ENABLE SYSCFG CLOCK
STR R1, [R0, #0]
LDR R0, =0x40013800 ; SYSCFG_MEMRMP
LDR R1, =0x00000001 ; MAP ROM AT ZERO
STR R1, [R0, #0]
LDR R0, =0x1FFF0000 ; ROM BASE
LDR SP,[R0, #0] ; SP @ +0
LDR R0,[R0, #4] ; PC @ +4
BX R0
and then prototyping this in C as
void Reboot_Loader(void);
I can step into it and at the end step into the code it branches to at 0x1ffff5138 which looks reasonable to my untrained eye.
0x1fff5132: 0x2000 MOVS R0, #0
0x1fff5134: 0x0af9 LSRS R1, R7, #11
0x1fff5136: 0x0000 MOVS R0, R0
0x1fff5138: 0xf000 0xf809 BL 0x1fff514e <<<<<<<<<<<<<<<<<<<<<<<<<< entry to bootloader?
0x1fff513c: 0x2800 CMP R0, #0
0x1fff513e: 0xd001 BEQ.N 0x1fff5144
0x1fff5140: 0xf7ff 0xffd0 BL 0x1fff50e4
0x1fff5144: 0x2000 MOVS R0, #0
0x1fff5146: 0xf7fb 0xf81f BL 0x1fff0188
0x1fff514a: 0xf000 0xf802 BL 0x1fff5152
0x1fff514e: 0x2001 MOVS R0, #1
0x1fff5150: 0x4770 BX LR
0x1fff5152: 0xf000 0xb801 B.W 0x1fff5158
0x1fff5156: 0x0000 MOVS R0, R0
0x1fff5158: 0x4607 MOV R7, R0
0x1fff515a: 0x4638 MOV R0, R7
0x1fff515c: 0xf7ff 0xff6a BL 0x1fff5034
0x1fff5160: 0xe7fb B.N 0x1fff515a
0x1fff5162: 0x46c0 MOV R8, R8
0x1fff5164: 0x46c0 MOV R8, R8
0x1fff5166: 0x46c0 MOV R8, R8
0x1fff5168: 0x46c0 MOV R8, R8
0x1fff516a: 0xf7ff 0xffe5 BL 0x1fff5138
0x1fff516e: 0xf7fd 0xb97f B.W 0x1fff2470
0x1fff5172: 0xf7ff 0xbf69 B.W 0x1fff5048
0x1fff5176: 0x1110 ASRS R0, R2, #4
Executing from that point results in a reset in several seconds.
Is this 'not working' or do I need to de-init the H/W to simulate a reset before calling that routine?
Thanks!
Edit: (Just found the edit button. 😉 )
Calling this as the first thing on main() does bring up the bootloader so it must be something to do with the subsequent H/W init. I suppose the best way to handle this is to set some flag (RTC backup register?) and reset then test and call immediately on entry to main.
2015-07-10 01:15 PM
; Quick IAR blind port
; Placed in startup_stm32f4xx.s after Reset_Handler,
; ideally called from there as magic number reset.
; In C defined as extern void Reboot_Loader(void);
; called as Reboot_Loader();
PUBLIC Reboot_Loader
SECTION .text:CODE:NOROOT:REORDER(1)
Reboot_Loader
LDR R0, =0x40023844 ; RCC_APB2ENR
LDR R1, =0x00004000 ; ENABLE SYSCFG CLOCK
STR R1, [R0, #0]
LDR R0, =0x40013800 ; SYSCFG_MEMRMP
LDR R1, =0x00000001 ; MAP ROM AT ZERO
STR R1, [R0, #0]
; LDR R0, =0x1FFF0000 ; ROM BASE
LDR R0, =0x00000000 ; OR GENERICALLY MAPPED AT ZERO
LDR SP,[R0, #0] ; SP @ +0
LDR R0,[R0, #4] ; PC @ +4
BX R0
; sourcer32@gmail.com
To better understand the context review this thread
/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Threaded.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Jump%20to%20internal%20bootloader&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=1653
2015-07-10 01:20 PM
2015-07-10 03:14 PM
Many thanks for your help, Clive.
And I'm not an assembler guy. 😉 But I did manage to get this to work. Unfortunately it only works if called before SystemClock_Config() in main (HAL/Cube libraries) so I'm trying to figure out how to set a flag somewhere that the app can test/clear on the nest reset. But that's a topic for another thread. ([DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Set%20a%20flag%20to%20test%20after%20reset&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx¤tviews=0]another thread)Thanks!2015-07-10 04:33 PM
Well the premise of the 5 year old thread I cited is that you write a magic valid in RAM, reset/restart the STM32 and during the Reset Handler it kicks directly into the ROM in close to reset conditions, and you avoid all the nonsense about clocks, plls and interrupts.