cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Timer XOR function TI1S bit, clarification

tomaskrueger
Associate II
Posted on July 11, 2014 at 22:03

Bonyour,

0690X000006058dQAA.png

I am refering to the STM32F2xx Ref manual, Timer, XOR function (also known as Hall Sensor Interface) asto above picture-extract on page

I try to understand.

We have the 3 Timer inputs CH1,2 and 3 each going to its dedicated input-signal-conditioner.

On CH1 there is an XOR Gate whos inputs connect to CH1,2 and 3.

(Is that a real XOR-Gate or just an OR-Gate??)

Its output goes to an ??-Gate that also accepts the original CH1 signal.

What Logic Gate would that be?...OR-gate?

As i understand, the TI1S-bit would switch the XOR-Gates output to the ??-Gate input.

My desired APP was to use CH1 as a clock input.

CH2 and CH3 receive a Gate-signal that shall inhibit the CH1 clock when they are high.

(XOR function)

But it does not seems to work.

Has anybody experience with this XOR functionallity?

1 REPLY 1
Posted on July 11, 2014 at 23:02

Its output goes to an ??-Gate that also accepts the original CH1 signal. What Logic Gate would that be?...OR-gate?

 

MUX one of the inputs is feed to the output based on some register selection (TI1S bit in the TIM_CR2 register)
Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..