cancel
Showing results for 
Search instead for 
Did you mean: 

Cube bug when assigning NOR flash??

jasonp4113
Associate II
Posted on May 20, 2014 at 01:11

Hi all

STM32F205 and cube 4.2.0

When assigning NOR flash, it does not matter which bank (chip select) you assign

&sharpdefine NOR_MEMORY_ADRESS        ((uint32_t)0x60000000)

always remains at 0x60000000 which is the wrong address if using anything other than nE1

Bug??

Thx

#stm32cube #nor #flash
1 REPLY 1
Posted on May 20, 2014 at 17:37

Hi,

We have already the limitation in the STM32CubeF4 FW bugs list, and it will be fixed in next release of F4 (early July). 

Thanks for the report.

With regards.