cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F071CB

entwicklung
Associate II
Posted on August 07, 2014 at 12:20

Hi,

I already got a project working based on the STM32F030 and with Keil MDK.

I based the project on a sample, so it was easy to get a working project.

This time I don't have a discovery board with the STM32F071 and there are no samples.

The startup file for this device is also missing.

I tried the stm32f0xx.s, but I'm not sure if its ok.

Do you have any advices how to get a working project for this device?

5 REPLIES 5
Amel NASRI
ST Employee
Posted on August 07, 2014 at 12:47

Hi Steffen,

You can start using the 

http://www.st.com/web/en/catalog/tools/PF260612

and generate your initialization code based on used device.

If you want to use the

http://www.st.com/web/en/catalog/tools/PF257884

, please refer to the examples inside it where you find all required files.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

entwicklung
Associate II
Posted on August 07, 2014 at 12:54

Hi Mayla,

I want to use the standard library.

There are no files specific to stm32f071.

It looks like there are only files for  STM32F030, STM32F031, define STM32F051, STM32F072 and STM32F042.

I am a little bit confused at this point

entwicklung
Associate II
Posted on August 08, 2014 at 10:25

Hey, I still have problems to get a working project with my STM32F071CB.

Where can I find the startup files and header for different devices? All I got from the library is this:

#if !defined (STM32F030) && !defined (STM32F031) && !defined (STM32F051) && !defined (STM32F072) && !defined (STM32F042)
/* #define STM32F030 */
/* #define STM32F031 */
/* #define STM32F051 */
#define STM32F072 
/* #define STM32F042 */
#endif

Amel NASRI
ST Employee
Posted on August 08, 2014 at 12:06

Hi Steffen,

Please note that STM32F071 is the same as STM32F072 where only USB & CAN were removed.

So there is no problem to use the STM32F072 FW on STM32F071 products.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

entwicklung
Associate II
Posted on August 11, 2014 at 08:43

Thanks a lot. This answer helps!

I wasn't sure about it's family line. I thought it was more familiar with the 51.