cancel
Showing results for 
Search instead for 
Did you mean: 

STSW-CONNECT009 program for SPIRIT1 won't open

jasongao
Associate
Posted on June 12, 2014 at 01:03

Hello,

I'm evaluating the SPIRIT1 transceiver with the ''STEVAL-IDS001V5'' evaluation kit.

After installing the ''STSW-CONNECT009'' version 1.0.7

software, it does not launch when I click on the shortcut, it just

briefly turns the mouse cursor into a progress circle, and then

nothing happens.

I have tried installing the software on:

Windows 8.1 64-bit

Windows 8 64-bit

Windows 7 32-bit

And have tried the various compatibility modes and ''Run as

Administrator'', and nothing has worked.

(The STEVAL-IDS001V5 USB hardware works fine, it shows up as a COM

port in Windows after installing the drivers. This seems to be purely a problem

with the software included with it).

Has anyone else encountered this issue and found a solution?

Thanks!
1 REPLY 1
jasongao
Associate
Posted on June 12, 2014 at 06:23

Hello,

I figured out the problem, here is the description and solution to save time for anyone else who encounters the same problem:

Solution:

Install the Microsoft Visual C++ 2005 Runtime from:

http://www.microsoft.com/en-us/download/details.aspx?id=3387

Problem:

ST incorrectly includes the Microsoft Visual C++ 2008 Runtime DLLs with the program, however, the program actually needs the Microsoft Visual C++ 2005 Runtime DLLs. A lot of people who already have the correct runtime installed (from using other programs previously) will not run into this issue. I, however, had created several clean installations across multiple versions of Windows and could never get it to work, precisely because the wrong Visual C++ runtime was included, and the correct one had never been installed on the system before.

I hope ST will more carefully test their programs in the future, I was about ready to give up on evaluating the SPIRIT1 RF transceiver.