2014-11-18 07:14 AM
Dear All,
It would be much appreciated, if some one can give me a video links that explaining each every step of operation of STM 32F0 TIM2 or any timer Thanks in advance2014-11-18 07:32 AM
Maybe somebody does provide that; but meantime, what about the old fashioned reading, of the relevant chapters of Reference Manuals, and AN4013?
JW2014-11-18 07:41 AM
2014-11-18 07:42 AM
Dear JW,
That truth but I think video presentation will help to more understand reading2014-11-18 08:11 AM
A lot of us don't have the time/patience to produce videos, so what exactly with the timers are you having a problem getting your head around?
The timers effect division of an input clock source, this is done with counting and comparison elements. In input modes the channels can latch the content of the primary counting element, time stamping the input against the ticking time base. In output modes the comparators are using the channel latches and the ticking time base, and can generate signals/interrupts/triggers when the two match, or exceed. What other microprocessors, timers, or electronics, do you currently have familiarity with? Perhaps this context will allow for a better tailoring of a response. In this profession you're going to have to master the reading of technical documentation. If you're a visual guy, look at the illustrations.