cancel
Showing results for 
Search instead for 
Did you mean: 

Crystal Gmcrit for STM32F401

ChrisFyberLabs
Associate II
Posted on July 03, 2014 at 10:25

Hi, I am trying to source smaller crystals (~2520) for USB support on the STM32F401.  The best I can find so far is 1.5mA/V.  I am calculating based on the information in AN2867 and the datasheet not mentioning Gm(as AN2867 requests), but a Max Gmcrit of 1mA/V.  I assume that the max is a hard number and I am interpreting the table Table 37. HSE 4-26 MHz oscillator characteristics in the datasheet correctly.  Would 12 or 16Mhz crystal still drive USB OK?  I don't believe any other feature on the chip requires an ext crystal.

0 REPLIES 0