cancel
Showing results for 
Search instead for 
Did you mean: 

LSM303C

daschenbrenner
Associate II
Posted on July 07, 2014 at 15:40

Hi all,

I am working with the LSM303C and with the EVALBoard ST8S003VLDISCO.

When i want to access the Magnetometer data it is giving me some strange values.

The Values of the High-Byte are staying constant always with the same values while the Low-Bytes are jittering a lot - not reacting to an external magnet.

I can say that the I2C is working properly, because i am able to read and write registers.

The Sensor is also working. I`ve tested it with another system.

I tried several configurations that work with an Arduino and M3 Board from NI - but it doesnt work.

Do you know what this could be?

The Accelerometer works properly

Regards

Asche
0 REPLIES 0