cancel
Showing results for 
Search instead for 
Did you mean: 

STR9 - Inrush current on the VDD supply

jtual
Associate II
Posted on July 29, 2014 at 16:52

Hi,

I have a issue with the power supplies of my electronic board at start up of microcontroller STR912FAW47. Someone know the inrush current of microcontroller on VDD (1,8V) and VDDQ (3.3V) at power on?

With an oscilloscope, it seems that the microcontroller starts to consume at the VDD treshold  of 0,7V because I have an inrush current when the VDD supply is above 0,7V.

Thanks,

Jerome

2 REPLIES 2
Posted on August 03, 2014 at 05:13

Do you have NRESET/NRST clamped to ground at this point?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
jtual
Associate II
Posted on October 08, 2014 at 12:04

No, the RST input is connected to pull up of 10K and a 100nF capacitor to the ground.