cancel
Showing results for 
Search instead for 
Did you mean: 

Usage Fault with STM32F7 HAL

imtiaz
Associate II
Posted on October 21, 2016 at 01:09

HI All,

If I enable usage faults in my F7Discovery project (F769) - I get usage fault in the HAL - specifically in stm32f7xx_hal_dsi.c line ♯ 1281

 hdsi->Instance->GPDR=((uint32_t)(*(ParametersTable + uicounter)) | \

                            ((uint32_t)(*(ParametersTable + uicounter+1)) << 😎 | \

                            ((uint32_t)(*(ParametersTable + uicounter+2)) << 16) | \

                            ((uint32_t)(*(ParametersTable + uicounter+3)) << 24));

My debug output from the hard fault handler is as follows:

Unaligned access UsageFault<\n>

r0  = 0x0800d541<\n>

r1  = 0x00000000<\n>

r2  = 0x00000039<\n>

r3  = 0x0000000e<\n>

r12 = 0x00000006<\n>

lr  = 0x08001cd1<\n>

pc  = 0x08001cf0<\n>

psr = 0x01000000<\n>

I would like to enable this for my project but this wont be possible if the libraries are faulting . The code is standard cube code provided by ST.

Any ideas on if this can be fixed ?

Thanks

Imtiaz

#stm32f7
0 REPLIES 0