cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F427VI + STemWin + RA8875

ertanaldogan
Associate II
Posted on August 06, 2014 at 11:49

Hello, I have a problem for driving LCD. Let me tell you about hardware first:

- I am using STM32F427VI, 

- I am using FMC for communicating. D0..D15 and A16 and NE1 pins.

- Pin connections made for 8080 mode.

- I am not using an extarnal memory (ram or rom)

About software:

- I created project file with STM32CubeMX with last versions of F4 package.

- I copied STemWin 5.24b library from STM32CubeF4 folder. I created code without FreeRTOS version.

- I modified GUIConf and LCDConf files. Also i add a function for status reading. This is necessary for emWin for using with RA8875.

- I allocated about 192kbyte ram for emWin.

I am working on it about since 4 days. I can write to screen any message. I can draw to screen lines. But i cannot change background color, or i cannot draw a window. I can just write text messages and draw a line.

What is the problem you think? 

Do you thing, do not use an external ram is a reason for this? Because i dont use an external ram but almost in all examples an external ram is using.

#stemwin
0 REPLIES 0