cancel
Showing results for 
Search instead for 
Did you mean: 

FOC 4.0 for STEVAL-IHM039V1 - dualdrive

kovac
Associate II
Posted on October 29, 2014 at 11:24

Hello

This is just an information for the developers and the rest of people.

I'm working right now with STEVAL kit IHM039V1 for dual motor. I found that LCD code works only for single drive. Problem is probably in wrong file that is distributed with FOC library 4.0. Both hex files have the same size - see attached picture.

I solved this issue by compiling LCD project my self. But there was another problem with wrong definition of MCU constant for compiler - see attached file. It was STM32F40X. I had to chang it to STM32F40XX to compile the project without errors.

Daniel

#foc-4.0-dual
2 REPLIES 2
Gigi
Senior
Posted on December 12, 2014 at 11:45

I'm taking note for next release.

Thank you Daniel

Ciao

Gigi

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards