2014-09-19 04:19 AM
Hello friends.
I'm trying to communicate with DS18B20 via 1-wire interface.
Here is the example of reset function (all pins and clk are set erlier). The problem is that the variable data
does not receive UART7 DR value. I use EWARM. I see that DR receives the response from the DS18B20. Is this
some compiler options?print_number (data) � prints 3 digit number on the LCD. In this function it is always 255, however data
variable is unavailable in the watch window.
void ow_reset()
{
USART_InitTypeDef USART_InitStructure;
uint16_t data;
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_Init(UART7,&USART_InitStructure);
USART_Cmd(UART7,ENABLE);
USART_ClearFlag(UART7, USART_FLAG_TC);
USART_SendData(UART7, 0xf0);
data = USART_ReceiveData(UART7);
while(USART_GetFlagStatus(UART7, USART_FLAG_RXNE) == RESET);
while (USART_GetFlagStatus(UART7, USART_FLAG_TC) == RESET);
print_number (data);
}
#debugger-is-invasive #1-wire2014-09-19 05:11 AM
2014-09-19 09:12 AM
I tried with and without that function - nothing changed. It is important that UART7 DR is 0xE0 and equals the response value of ds18b20...
What is interesting when I changed data = USART_ReceiveData(UART7); with data = (uint16_t)(UART7->DR & (uint16_t)0x01FF); correct value started to be indicated on the lcd, but still in the watch expression window the value of data is unavailable2014-09-19 09:28 AM
USART routines often fail when you try to step through them using a debugger, which reads out the state of USART's registers (to be able to display them) at every step. This is because some of the status flags are cleared by hardware upon reading the registers, e.g. the RXNE flag is cleared when the DR register is read.
JW2014-09-19 09:55 AM
You can't simply park a debug view over peripheral registers and hope to get a realistic view of them. The debugger is invasive, and if you want to know what's happening internally you need your own code to read the registers, output diagnostics, and react to the transient state and interplay of the registers appropriately.
2014-09-19 12:56 PM
''It is important that UART7 DR is 0xE0 and equals the response value of ds18b20''
Have you read this:http://www.maximintegrated.com/en/app-notes/index.mvp/id/214
?And have you got your hardware connections correct?The 0xE0 is not the ''response value'' from the DS18B20 - it is just the effect of the Presence Pulse.And it is not guaranteed to be 0xE0...2014-09-19 10:22 PM
''USART routines often fail when you try to step through them using a debugger...''
Yes, I tried step by step debug...it was a mess. So I put the breakpoint at the very end of the function.2014-09-19 10:25 PM
''You can't simply park a debug view over peripheral registers and hope to get a realistic view of them. The debugger is invasive...''
I started to print certain information on the LCD. For example this substitution data = USART_ReceiveData(UART7); with data = (uint16_t)(UART7->DR & (uint16_t)0x01FF); I could catch only with the LCD. However it seems that it should be the same action.2014-09-19 10:33 PM
''Have you read this:
http://www.maximintegrated.com/en/app-notes/index.mvp/id/214
? And have you got your hardware connections correct? The 0xE0 is not the ''response value'' from the DS18B20 - it is just the effect of the Presence Pulse. And it is not guaranteed to be 0xE0...'' Yes, exactly this article I used as a reference. The part from this article: ''A single slave device running at minimum internal timing will change the response to 0xE0. A single slave running at maximum internal timing will change the response to 0x90. '' I hope the one DS18b20 I use is running at minimum timing 🙂2014-09-19 11:51 PM
''I hope the one DS18b20 I use is running at minimum timing''
But ''hoping'' does not make it so!Statistically, it is highly unlikely to be at either the maximum or minimum limits - or any other specific value, for that matter!