cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L052 changing battery

baev_al
Associate II
Posted on July 30, 2015 at 08:50

Hello friends.

I'am working on a project using STM32L052 and Nokia5110 display. It is a temperature controller. It will utilize RTC. It will work from two AA batteries.

The question is what is the best way to change the batteries (two AAs) so that it would not be necessary to set RTC after this change.

Is there any solution without additional battery?

Thanks.

1 REPLY 1
oliver239955
Associate II
Posted on August 03, 2015 at 09:09

Hi Alexander,

I got the same problem. It is a great pity, that there is no external battery input for the STM32L0. Because of this I had to change to an external RTC, which I power from a big capacitor, when there is no battery plugged.

I am also open for a better solution!

Greets