2014-08-20 11:00 AM
Maybe this is explained somewhere in the RM, but because I didn't find the answer with a brief study I will try if the forum can help...
So the question is about the alternate function pin named TIM2_CH1_ETR. I want to use this pin as the second interface to an incremental encoder (the other is TIM2_CH2), but this extra ETR suffix confuses me a bit. If I understand correctly ETR stands for external trigger, which actually I don't need in my application. So somehow the ETR function and normal TIM2_CH1 capture input are multiplexed to the same pin, but is it possible to configure the timer such a way that the ETR function is not used?2014-08-20 11:05 AM
2014-08-20 11:39 AM
Hi Clive,
And thanks for the prompt reply! Just to clarify, as I already use CH1 in input mode, but I can configure the timer such a way that ETR doesn't affect the operation, right?2014-08-20 02:06 PM