2015-08-30 10:49 PM
hi every body
i have a problem with strstr function, i receive characters from uart with interrupt & save them on the n length array(buffer array), then in main loop i check buffer with strstr function from string.h for finding a special arrayof characters(for example'' hello''),it works fine for the first time but some time it dosent work and without receiving that array of string it act like when find matching. sample code : interrupt handler ,when character received,it save that in the buffer:Code:
void USART1_IRQHandler(void)
{
/* RXNE handler */
if(USART_GetITStatus(USART1, USART_IT_RXNE) != RESET)
{
Rx_Buffer[Counter_Num1]=(char)USART_ReceiveData(USART1);
Counter_Num1++;
if(Counter_Num1==100)
{
Counter_Num1=0;
}
}
}
main loop:
in some primary matching it works fine (when i type ''hello'',it return ''1234'') but after some tries it permanently return ''1234'' without matching
while(1)
{
//--------------------------------------
do
string_pointer = strstr (Rx_Buffer, ''hello'');
while(string_pointer==NULL);
USART_SendData(USART1, '1');
delay_ms(50);
for(loop_counter=0;loop_counter<100;loop_counter++)
{
Rx_Buffer[loop_counter]=' ';
}
string_pointer=NULL;
USART_SendData(USART1, '2');
delay_ms(50);
USART_SendData(USART1, '3');
delay_ms(50);
USART_SendData(USART1, '4');
delay_ms(50);
//-----------------------------------
}
i used stm32 & keil
thanks for any help
2015-08-31 12:37 AM
Hello,
If Rx_Buffer is not well itnialized to zero (even if it is not), it should be safer to use strnstr i think:string_pointer = strnstr (Rx_Buffer, ''hello'',
sizeof(Rx_Buffer)
);But i'm not sure this is the issue 🙂Aurélien2015-08-31 05:18 AM
String functions are VERY sensitive to the strings being properly NUL terminated. Otherwise the operations are unbounded.
Also WAIT for TXE before using USART_SendData(), it's the way to KNOW the buffer is empty so it's ready to accept a new character, and you don't need arbitrary software delays.