cancel
Showing results for 
Search instead for 
Did you mean: 

ADC and interrupt in motor control

cnmountain
Associate II
Posted on February 07, 2015 at 05:05

The original post was too long to process during our migration. Please click on the attachment to read the original post.
3 REPLIES 3
hassanbhutta91
Associate II
Posted on February 07, 2015 at 06:18

hye, are you using motor control library?

cnmountain
Associate II
Posted on February 09, 2015 at 16:18

I am not sure if this belongs to ST motor control library, but I am creating my project from this example project in the library

\STM32Cube_FW_F0_V1.1.0\Projects\STM32F0308-Discovery\Examples\TIM\TIM_ComplementarySignals

Gigi
Senior
Posted on March 20, 2015 at 17:01

Ciao

You can find the Motor Control Library

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1734/PF257936?s_searchtype=partnumber

The problematic to synchronize the ADC sampling with the PWM period is covered, but in the WEB site you can find only the compiled version so you need to ask for the source code to your nearest ST support office.

Otherwise you can ask this to the STM32 forum.

Ciao

Gigi