2014-09-25 01:36 PM
Hi all,
After reading the RCC_CSR register to determine the reset source, I want to clear the register so as to be able to resolve future non-por resets. When I follow the instructions in the datasheet, the bits do not clear. Here is the code sequence that I use:RCC
->
CSR
|=
(1U <<
24
)
;
// RMVF : Clear reset flags
RCC
->
CSR
&=
~(1U <<
24
)
;
The data sheet is not clear on exactly how to use this bit. It says to set the bit, but does not specify if the bit will reset automatically or if it needs to be explicitly cleared afterward.I have tried both cases and still, the flags do not reset.Also, I am able to determine POR and SOFWARE reset, but when I drive the external reset pin, the PIN reset flag is not set.Has anyone else had this problem?I have looked at the errata for this device and the only thing related is a need for a work-around delay when enable the RCC clock.I suspect I am missing something and that somehow these bits a write-protected.Any hints, solutions, etc. would greatly by appreciated. #poor-quality-of-documentation #reset-id-flags-clear2014-09-25 11:47 PM
Quick experimentation (albeit on a STM32F4) revealed, that:
- the reset-source bits can't be written - the RMVF bit is auto-cleared, i.e. it's enough to write 1, and this cleared the reset bits for me Thus, I'd try RCC->CSR = 1 << 24; (or, more precisely, I'd do RCC->CSR = RCC_CSR_RMVF), but I honestly fail to see why wouldn't your sequence do the same. I did not experiment with the reset input. The documentation is hopeless. JW2014-09-26 03:33 AM
The Reference Manual RM0367 DocID025274 Rev 2 p189/897 says,
Bit 24 RMVF: Remove reset flag This bit is set by software to clear the reset flags. 0: No effect 1: Clear the reset flags That looks clear to me - where ''set by software'' means you do it, the hardware doesn't.2014-09-26 06:57 AM
2014-09-26 07:21 AM
The header files often have ''encoded'' bits, indexes and masks, so one shouldn't assume a one-to-one relationship between encodings the peripheral library utilizes with the bits in the registers as described by the Reference Manual.
Doing a RMW &= ~X isn't going to set desired bits to ONE2014-09-29 01:14 AM
> I found the problem and it is with the datasheet.
> The bit positions defined in the datasheet do not match those defined in the device header file. >When I use RCC->CSR = RCC_CSR_RMVF, it works. A bug in the RM indeed. Not the first one... :( JW2014-10-02 03:51 AM
A bug in the RM indeed. Not the first one... :(
In stm32l053xx.h file, RCC_CSR_RMVF value is ''0x00800000''. It corresponds to bit 24 of the reference manual.Am I wrong with RM bug you are reporting?-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2014-10-02 07:01 AM
In my calculator, when I type in 1<<24 , it results in 0x01000000... 😉
Jan2014-10-07 06:09 PM
The value in my header file is the correct one. It is the datasheet that shows the wrong bit position.
Cheers! Dan