2015-05-31 06:55 PM
I have serious problem.
I tried to write software to the devices with JTAG and Flash Loader Demonstrator,but both of them could not find device.I guess the device revision has something different with revision ''Z''.Revision ''Z'' devices are successful with JTAG and Flash Loader Demonstrator,however ''L'' are unsuccessful at all.If anyone know about this problem, please tell me tips.Following infomation was tried to write with JTAG and Flash Loader Demonstrator.--- Unsuccessful Device BGA Package---ARM LSTM32F407IEH6HPADX VQKOR HP 504--- Successful Device 1. BGA Package---ARM ZSTM32F407IEH6HPAFW VGKOR HP 322--- Successful Device 2. QFP Package---ST ZSTM32F407ZGT6ARM HPABUVGKORHP4L72015-05-31 08:28 PM
No particular insight.
Usual things to confirm : Voltages on VCAP pins State of NRST pin State of BOOTx pins2015-05-31 08:34 PM
Thank you, clive1
I rework device revision L to Z then the MPU connect with JTAG and Serial.(On some of same PCB bords.)So I worder why doesn't work this device.Everything same as revision L.2015-05-31 09:06 PM
Hi, clive1
>Voltages on VCAP pinsShould I connect BYPASS_REG pin to Low?Now, this pin is open.2015-06-08 12:16 AM
As the result, VCAP Pins Voltage is a Key!
Bypass_REG pin connect to the GND throuh 10k ohm, thenVoltage on VCAP is about 2.6V and confirm to write firmware.Now, Everything is OK.Thank you a lot.2015-06-08 06:25 AM
Shouldn't the VCAP pins be at 1.25V?! How have you got these parts wired up? (schematic)
2015-06-08 06:43 PM
Hello Clive
>Shouldn't the VCAP pins be at 1.25V?! How have you got these parts wired up? >(schematic)It was 1.25V. I made typo.Thanks.