2014-10-08 05:48 AM
Hello :),
I need
help
to solve the
communication between processor
C805and
BL module.
Devices communicate
via
UART
(serial
port -
>TX
/
RX
pins
)and I need
to do a basic
setup
.Then
send
it
AT
commnadsBL
module
.UART
is working
well
,and
after turn on
BL
moduleget an answer
AT
-AB
-CommandMode-
AT
-AB
BDAddress
BDR
But
when I send
some
AT
commands
are
unanswered.
I do not understand
the syntax
is respected
.. just
do not know
whether
statements end with
\
r
\
n
or
something
like that.
Or whether they are
poorly
chosen
AT
commands
in the communication.
Please help me 🙂 guys, tnx2014-10-08 08:35 AM
This isn't an 8051 forum, or one for this module. If the module is non-responsive you'd perhaps want to check the power, and signalling via a scope. That you've got the Tx/Rx sense right, and the baud rate and framing correct. If you are unfamiliar with functionality try connecting it to a PC first, use terminal applications there and then go embedded when you have more insight.