cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 FOC SDK & CubeMX

vromanov
Associate II
Posted on March 15, 2016 at 15:44

hi!

Can be STM32 FOC SDK & CubeMX generated code used in same project? We already have some libraries based on CubeMX. 

2 REPLIES 2
Gigi
Senior
Posted on April 01, 2016 at 15:13

Ciao Vladimir

No, is not possible at the moment because the FOC SDK is based on the standard peripheral library and the code generated by the CubeMX is based on CubeHAL.

We plan to converge the FOC SDK versus the CubeMX but this will not be ready very soon.

Ciao

Gigi

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards