cancel
Showing results for 
Search instead for 
Did you mean: 

STM8S003F3 reset pin - output frequency

vindhyachal
Associate II
Posted on February 27, 2015 at 07:24

1. I have made a circuit using STM8S003F3.

I don't understand somehow when I probe reset pin of MCU, it is giving 12Khz freq output.

Thus I am unable to program/debug the MCU.

2. I have removed everything else from board. Just +5V supply & MCU.

MCU supply is decoupled by 0.1u & 1u caps.

Vcap pins is decoupled by 1uF cap.

Reset pin is decoupled by 0.1uF cap.

That's it . Nothing else on circuit.

3. I have probed VCC pin of MCU, I get clean +5V across it.

Probing Vcap pin gives +2V clean.

I have also removed 0.1u cap from reset pin & then checked the bare pin but same result.

Edit: I have also changed 2 MCU but same results

0 REPLIES 0