cancel
Showing results for 
Search instead for 
Did you mean: 

Using SPI4 in STM32F429 - what are the changes needed

hariprasad
Associate III
Posted on February 08, 2015 at 15:08

I want to use STM429 MCU's SPI4 .

But when I checked stm32f4xx_rcc.h  it only provides upto 3 spi's gates.

How can I add support for SPI4 ?

What are the changes in the which files required inorder to achieve SPI4 working?

#spi #discovery #- #stm32f429
1 REPLY 1
Posted on February 08, 2015 at 16:38

What version of the library are you using?

The F429-DISCO v1.0.1 and F4 DSP v1.3.0 both reference SPI4

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..