cancel
Showing results for 
Search instead for 
Did you mean: 

Using SPI4 in STM32F429 - what are the changes needed

hariprasad
Associate III
Posted on February 08, 2015 at 15:05

I want to use STM429 MCU's SPI4 .

But when I checked stm32f4xx_rcc.h  it only provides upto 3 spi's gates.

How can I add support for SPI4 ?

What are the changes in the which files required inorder to achieve SPI4 working?

#stm32f429 #discovery #spi #!bug
1 REPLY 1
Posted on February 08, 2015 at 16:59

[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Using%20SPI4%20in%20STM32F429%20-%20what%20are%20the%20changes%20needed&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx&currentviews=5]Cross-Post

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..