cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32 Nucleo L152RE and low power configuration

antonio23
Associate II
Posted on July 30, 2015 at 16:36

Hi to all, i use stm CubeMX with HAL library and Keil now i want develop  the low power configuration on my Nucleo  stm32L152RE, can you see a example or other information?

can you help me?

best regards

A.
1 REPLY 1
Amel NASRI
ST Employee
Posted on August 13, 2015 at 13:02

Hi AntonioLinux,

Have a look to the set of examples available in STM32Cube_FW_L1_V1.3.0\Projects\STM32L152RE-Nucleo\Examples\PWR.

STM32CubeL1 package and some user manuals are available in

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1897/PF260821

.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.