2015-05-19 01:07 PM
Functions in usbd_cdc.c which return values of USBD_StatusTypeDef as defined in usbd_def.h (e.g USBD_OK) are defined as uint_8.
This causes IAR to issue ''enumerated type mixed with another type'' errors when properly typing variables to hold the return value of these functions. Yes, it is possible to cast the result to eliminate the warning, but the source should be corrected (IMNSHO).2016-12-18 02:39 AM
still not fixed so far (STM32CubeF1 1.7.0, 29.04.2016)
2017-01-13 09:24 AM
Hi
Katzenberger.Michael
,Could you please create a new thread detailing your issue.
This will help usin our investigation.
Khouloud.
2017-01-14 05:09 AM
done: