cancel
Showing results for 
Search instead for 
Did you mean: 

XPost: LSM6DS0 calibration and DPS values

aaron239955_stm1
Associate
Posted on February 09, 2015 at 17:51

Cross post from the gyro forum (didn't realize it was in the wrong spot).

Hi All, I need some advice/help getting my gyro calibration.  I'm using the X-NUCLEO-IKS01A1 board to evaluate the LSMDS0 gyro.

The raw data that's coming from the LSM6DS0 doesn't seem to be DPS, the values are much to high for the range specified in the data sheet.  Is there some formula I have to apply to it?

Also, I'm prepping the code and documentation for our production team to use the LSM6DS0 in their product, but the calibration routine will have to be done.  There are several documents provided by STM that outline the technique required for calibration after the LSM6DS0 is mounted on the IC and installed in the device.     But I haven't found one exactly for the LSM6DS0.

TLDR: I need help setting up the calibration and DPS value calculation for the LSM6DS0.

Thanks!

#lsm6ds0-iks01a1-calibrate-dps
1 REPLY 1
aaron239955_stm1
Associate
Posted on February 10, 2015 at 16:26

Anyone? Wow, this forum is a ghost town....