cancel
Showing results for 
Search instead for 
Did you mean: 

STM32Cube_FW_F4_V1.16.0 demos for F469 discovery don't work using IAR

Goguey.Pascal
Associate II
Posted on September 14, 2017 at 06:57

Hello!

Basically the title explains all. Here are a few details.

I'm using IAR 8.11, and I'm trying to compile sample code from STM32Cube_FW_F4_V1.16.0, with the board I have: a STM32469I-Disco. I tried to compile all the examples related to LCD, none of them works. I was told it's probably a problem in STM32Cube_FW_F4_V1.16.0 which should be use with IAR 7. I was told that 7.8 works.

Will there be an update to these firmwares (V1.17 for example) anytime soon?

Best regards,

R

1 REPLY 1
Posted on September 14, 2017 at 08:01

You might want to ask yourself why 8.x is incompatible with prior releases, and what else in your code base this might affect adversely. Does IAR provide a compatibility mode/setting?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..