cancel
Showing results for 
Search instead for 
Did you mean: 

Can I use External interrupt Pins for Wakeup?

nooshin_1382
Associate II
Posted on August 08, 2015 at 14:27

Hi

I want to use External IRQ Pins for Wake up , Can Use These interrupts or not ?

ex : EIRQ0

Best Regards

Nazerian Vanima
4 REPLIES 4
ssk
Associate II
Posted on August 10, 2015 at 07:00

Hello,

Which power down mode you are using? Based on power down mode used, the exit sources are different. Refer section #8.1.3 of reference manual.

As for using external interrupt, you need to use wakeup module (corresponding wakeup pin) for exiting the stop and standby power down mode.

Regards,

Mike.

nooshin_1382
Associate II
Posted on August 10, 2015 at 07:41

Hi Mike

Thanks for your response

I use the STANDBY mode for going to sleep and use wake up pins for gonig to DRUN mode but my problem is the SPC560B50L5 have 19 Wakeup pins and i need 25 Wakeup pin because of this issue i think about external interrup .

according to Refrence manual i think the MCU did'nt wakeup with external interrupt 

Best Regards

Nazerian Vanima

ssk
Associate II
Posted on August 10, 2015 at 07:49

Yes, wakeup is not possible with external interrupt pins. Instead you can try some decoding logic using available wakeup pins.

Best Regards,

Mike.

Erwan YVIN
ST Employee
Posted on August 10, 2015 at 16:46

Hello Vanima ,

From STANDBY mode, wakeup is not possible by EIRQ.

you should use WKUP Interrupt.

    Best regards

                 Erwan