cancel
Showing results for 
Search instead for 
Did you mean: 

TNeo: stable open source real-time kernel with well-formed code and detailed tests (for Cortex-M0/M0+/M3/M4/M4F)

secmail
Associate
Posted on January 02, 2015 at 15:56

I'd like to present real-time kernel:

https://bitbucket.org/dfrank/tneokernel

.

TNeo was born as a thorough review and re-implementation of

http://tnkernel.com

. The new kernel has well-formed code, inherited bugs are fixed as well as new features being added, it is well documented and tested carefully with unit-tests.

Currently it is available for the following architectures:

  • ARM Cortex-M cores: Cortex-M0/M0+/M1/M3/M4/M4F (supported toolchains: GCC, Keil RealView, clang, IAR)
  • Microchip: PIC32/PIC24/dsPIC

Comprehensive documentation is available in two forms:

Short list of features can be found

http://goo.gl/dDFAUJ

.

#kernel
1 REPLY 1
secmail
Associate
Posted on March 17, 2015 at 00:34

TNeo v1.07 is released, this is a minor release with a few bugfixes and some new features.

Changelog is available here:

http://dfrank.bitbucket.org/tneokernel_api/dev/html/changelog.html

Downloads here:

http://bitbucket.org/dfrank/tneokernel/downloads