cancel
Showing results for 
Search instead for 
Did you mean: 

HT221 functional failure for above humidity sensor after long duration exposure to the air

jason239955_st
Associate III
Posted on December 15, 2017 at 17:24

Hi Sir/Mdm,@

Please advise how many heating cycle can withstand by HTS221 humidity sensor? 

Can we proposal to heat the sensor for 2nd time at 80 degree?

Regard's

Jason

1 REPLY 1
Miroslav BATEK
ST Employee
Posted on December 16, 2017 at 11:09

What you mean by heating cycle? Usign internal heating element or heating by some external source?

The sensor operates over a temperature range from -40 °C to +120 °C, so heating to 80 °C will not hurt the sensor.